MITSUBISHI ELECTRIC Changes for the Better
Volver al resumen
Compartir a través de
Water / Waste Water

Digitalisation of water infrastructure

24.07.20263 minutos de lectura

The global digital water industry is undergoing a profound transformation. As water scarcity intensifies, regulatory requirements tighten, and operational budgets shrink, relying on legacy, manual workflows is no longer a viable option for utilities. Modern water and wastewater systems must adopt advanced water management technology to secure long-term operational resilience, optimise resource consumption and protect critical public infrastructure.

Introduction to the digitalisation of water infrastructure

Transitioning to a modern digital water infrastructure allows municipal and industrial operators to gain full visibility over highly complex, distributed networks. By deploying connected sensors, high-performance edge controllers, and centralised visualisation platforms, utilities can manage the entire water cycle seamlessly. This digital shift enables faster leak detection, automated process adjustments, and proactive resource conservation, ensuring that clean water is delivered safely and efficiently to growing urban and industrial areas.

Why aging water infrastructure can no longer run on manual processes?

Many water networks rely on infrastructure that has been in operation for decades. Over the years, selective, section-by-section upgrades have led to extreme system complexity and severe interoperability issues between different equipment brands. Manual tracking and physical inspections cannot keep pace with these challenges, nor can they detect hidden capacity issues or slow-developing leaks.

To prevent catastrophic breakdowns and water loss, utilities must prioritise water utility digitalisation. Integrating legacy assets with modern platforms using open communication protocols like OPC UA and MQTT allows operators to harvest critical data without replacing functioning hardware. This backwards-compatible migration path minimises upfront capital expenditure while providing a clear roadmap for systematically upgrading your plant.

Where energy waste actually happens in water treatment facilities?

Water and wastewater treatment are notoriously energy-intensive processes, often ranking among the highest operational expenses for municipalities. Significant energy waste occurs in multi-stage pumping stations and aeration systems that run continuously at fixed speeds, regardless of actual demand or fluctuating flow rates.

Implementing energy optimisation in water systems is critical to stopping this waste. By pairing high-efficiency electric motors with smart variable speed drives (VFDs) and dedicated energy monitoring software like EcoAdviser, facilities can identify underperforming assets in real time. This setup allows the system to dynamically adjust motor speeds to match actual network pressure and demand, eliminating unnecessary power draw and significantly lowering greenhouse gas emissions.

From reactive to predictive: how automation changes wastewater operations

Traditional maintenance strategies in the water sector have historically been reactive - responding only after a pump fails or a pipe bursts. Transitioning to predictive maintenance water treatment completely changes this dynamic by focusing on malfunction precognition.

By utilising smart frequency inverters equipped with built-in diagnostic tools, operators can monitor the physical health of machinery continuously. For instance, an increase in vibration amplitude can indicate a worn bearing, while electrical anomalies can signal early-stage corrosion. Detecting these deviations in real time allows maintenance teams to schedule repairs during planned shutdowns, eliminating unplanned downtime and ensuring uninterrupted service for the community.

The technologies behind smart water infrastructure - and what each one does

Building a modern, resilient water network requires a highly integrated stack of robust hardware and intelligent software. Similar to the advanced automation principles deployed in the first sustainable metal recycling plant, a smart water system relies on several key technological layers:

  • Edge & Control Layer: High-performance MELSEC programmable logic controllers (PLCs) execute precise, localised control loops for chemical dosing, filtration, and flow regulation.

  • Visualisation Layer: The ICONICS GENESIS 11 SCADA platform unifies data from multiple systems into intuitive, real-time dashboards accessible on any device.

  • Data Archiving Layer: Hyper Historian, an advanced 64-bit high-speed data archive, securely logs massive streams of historical and telemetry data for reporting and compliance.

  • Drive Layer: FREQROL variable speed inverters optimise motor efficiency while performing automatic self-diagnostics.

Real-time data and IIoT: from sensor to decision in water management

Deploying IIoT in water management bridges the gap between isolated field devices and high-level executive decisions. Connected sensors across the network continuously capture parameters such as flow velocity, pressure, pH, and turbidity.

This data is processed at the edge and transmitted to the central GENESIS 11 platform, transforming raw telemetry into actionable insights. This seamless flow of information enables operators to make data-driven decisions instantly, which directly boosts overall plant performance, simplifies regulatory reporting, and ensures strict compliance with environmental safety standards.

What wastewater automation looks like in practice?

In practical applications, smart wastewater systems utilise advanced wastewater treatment technologies to automate highly complex biological and chemical cycles. By integrating a digital twin water infrastructure, operators can create a virtual model of the physical plant to simulate different operational scenarios, such as sudden capacity surges during heavy rainfall or storm sewer overflows.

This predictive capability enables highly optimised smart wastewater management, allowing automated systems to adjust valves, pumps, and aeration blowers dynamically. Furthermore, by adopting a gradual, step-by-step implementation approach using the Smart Manufacturing Kaizen Level (SMKL) methodology, utilities can digitalise their operations incrementally, minimising investment risks while continuously improving efficiency.

What is the digitalisation of water infrastructure?

The digitalisation of water infrastructure refers to the integration of modern digital technologies - such as IoT sensors, programmable logic controllers (PLCs), high-speed data historians, and advanced SCADA visualisation software like GENESIS 11 - into water and wastewater networks. This process transitions traditional, manually operated facilities into highly connected, data-driven systems. Digitalisation allows utilities to monitor water quality, pressure, and flow rates in real time, automate routine processes, and proactively manage assets to prevent failures and optimise resource consumption.

How does wastewater automation reduce operational costs?

Wastewater automation reduces operational costs by eliminating inefficiencies in energy, chemical usage, and labor. By automating processes like aeration and pumping, the system dynamically adjusts equipment speeds based on real-time demand rather than running them at constant, maximum capacity. Furthermore, automated diagnostics identify equipment wear early, preventing expensive emergency repairs and unplanned downtime. Automated reporting also reduces the manual labor required for compliance tracking, allowing the existing workforce to focus on high-value optimisation tasks.

What role does IIoT play in smart water infrastructure?

The Industrial Internet of Things (IIoT) acts as the nervous system of smart water infrastructure. It involves deploying a network of connected sensors and smart devices across treatment plants, reservoirs, and piping networks. These devices continuously collect critical environmental and operational data, such as water temperature, pH, turbidity, flow velocity, and vibration levels. This data is transmitted securely to edge controllers and centralised SCADA platforms like GENESIS 11, enabling real-time monitoring, automated control loops and deep data analytics.

How does digitalisation improve energy efficiency in water treatment?

Digitalisation improves energy efficiency by providing complete visibility into where and when energy is consumed. Utilising dedicated energy management software, such as EcoAdviser, alongside smart variable speed drives (VFDs) like FREQROL, allows utilities to monitor the specific power draw of individual pumps and blowers. The system can then automatically adjust motor speeds to match actual network demand or shift energy-intensive operations to off-peak hours, significantly reducing overall electricity costs and carbon emissions.

What are the biggest barriers to digitalising water infrastructure?

The most common barriers include cybersecurity concerns, the complexity of integrating legacy equipment, and budget constraints. Because water systems are classified as critical infrastructure, they are prime targets for cyber threats, requiring robust "Defense-in-depth" security frameworks certified under IEC 62443-4-1. Additionally, many utilities operate with aging, fragmented systems that do not easily communicate with modern software. Overcoming this requires open communication protocols and a step-by-step migration strategy to minimise upfront risks and costs.

How do predictive maintenance systems work in water treatment facilities?

Predictive maintenance systems utilise advanced sensors and built-in artificial intelligence to monitor the physical health of machinery in real time. For example, sensors on a pump can detect slight increases in vibration amplitude or temperature, which are early indicators of a worn bearing. Similarly, smart frequency inverters can diagnose environmental issues like corrosion or electrical faults. The system alerts maintenance teams to these anomalies, allowing them to schedule repairs during planned shutdowns before a catastrophic failure occurs.

What is the difference between water automation and smart water management?

While water automation focuses on local, machine-level control - such as a PLC automatically opening a valve when a tank reaches a certain level - smart water management represents a holistic, enterprise-wide approach. Smart water management integrates local automation with high-level data analytics, SCADA visualisation platforms like GENESIS 11 and predictive modeling. It uses historical and real-time data to optimise entire distribution networks, manage water resources sustainably, predict future demand and make high-level strategic decisions.

What should water facility operators prioritise when starting a digitalisation project?

Operators should prioritise a gradual, step-by-step implementation strategy rather than attempting a complete, high-risk system overhaul all at once. Utilising methodologies like the Smart Manufacturing Kaizen Level (SMKL) model, facilities can start by digitalising a single machine or a small section of the plant. This approach minimises initial investment risk, allows the team to gain valuable experience, and provides clear, measurable results that make it easier to justify and plan future expansion phases.


Los temas

Water / Waste Water